Part Number: TMS320F28388D
Other Parts Discussed in Thread: C2000WARE
Tool/software:
Hello Supports Team,
I have the test setup based on the example provided by TI: generateNonMasterCLAReadViolation from C2000Ware_4_01_00_00\libraries\diagnostic\f2838x\examples\sdl_ex_ram_access_protect.c.
In the linker script, i have the ls6Data linked in LS0, and LS0 is set to CPU only. LS1 has the .scratchpad and set to CLA data. LS5, LS6, LS7 is set to CLA programm, Cla1Task1 has run address in LS5.
But during testing i notice the test only pass when in debugging session, when i unplug the debugger, power cycle the HW, attach the debugger again, i see the test failed.
What can be the reason?
Thanks.
BR
Chao