Tool/software:
Hi Expert,
My customer used to use BIOS as below, in BIOS, there is able to use SWI_POST function to change hardware interrupt to software interrupt, which will run after hardware interrupt like SCI interrupt,
when the code run in SWI_POST, the priority of this software interrupt can be set to lower than other software interrupt, so the code run in SWI_POST is able to be interrupted nest by other hardware interrupt like ADC interrupt, or be interrupted nest by other higher level software interrupt.
Now BIOS is not support on F28P65x, they have to use freeRTOS, they are asking how to set software interrupt in FreeRTOS like SWI_POST function in BIOS? can you suggest a guideline for this function? thanks.