Part Number: TMS320F280039C
Tool/software:
I have used example 5 to establish can communication but its not working can anyone please help me out(im not geting any signal)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F280039C
Tool/software:
I have used example 5 to establish can communication but its not working can anyone please help me out(im not geting any signal)
Varun,
Can you describe what you have done so far on example 5? Just wanted to understand which part does not work for you. What kind of hardware are you using?
Joseph
CAN will not transmit if it detects that there is a dominant bit that is holding the bus low. Best way to observe the CAN transactions is to hook up a CAN analyzer (PeakCAN...etc) or another launchpad. Are you able to connect to any one of these?
Thanks,
Joseph
Varun,
Please describe exactly what you are doing in the test case. Example 5 can be used either as transmit or receive. How did you configure it? If used as transmit, you may not see any activity on the CANTX pin since node might be seeing the CANBUS to be low. If used as receive, you will only see activities in CANRX pin if a node is transmitting valid frames in the CANBUS after the transceiver. This is the reason that I was asking if there you have the option for connecting CAN analyzer or any other CAN node to the CAN bus.
Regards,
Joseph
Ok,ex5 by default is in transmit mode. You have already confirmed that you set the CAN pin GPIOs accordingly to match the launchpad transceiver. Take note of the following too:
- On launchpad, ensure that GPIO4 and GPIO5 are in the CAN position through switch S4. Also ensure that the CANH and CANL from J14 connect to the CAN bus of the working micro through its CANH and CANL terminals.
- Ex5 has the baudrate set to 500kbps. Check that the other receiving micro with a proven code is also set to 500kbps, otherwise communication will not happen.