Part Number: TMS320F28P650DH
Tool/software:
Hi
I can calculate one block CRC successfully and as I have understood from the documentation that incase of large memory we need to split it in <= 0xFFFF and the result becomes the seed of next block.
flash area is 0x30000 -2 (0x60000 -4 bytes) words. so I am giving 95 x 4096 bytes in for loop and rest 4092 after for loop. unfortunately with no success.
for(u16i = 0; u16i < 95; u16i++)
{
// myVCRC0_CRC.pMsgBuffer = (uint16_t *)u16DataPointer;
memcpy(u16Array, (const void*)u16DataPointer,sizeof(u16Array));/**/
myVCRC0_CRC.run(myVCRC0_Handle);
u16DataPointer+= (4096/2);
myVCRC0_CRC.seedValue = myVCRC0_CRC.crcResult;
}
myVCRC0_CRC.nMsgBytes = 4092;
memcpy(u16Array, (const void*)u16DataPointer, (sizeof(u16Array)));/**/
myVCRC0_CRC.run(myVCRC0_Handle);
thanks and best regards