Part Number: TMS320F280039C
Other Parts Discussed in Thread: C2000WARE
Tool/software:
I am trying to operate the MCAN module on an F280039C MCU at 1 Mbps nominal and 5 Mbps data bit rates. I am having trouble spotting the correct settings to do so.
The MCAN module clock prescaler is set to 3.
![]()
I am able to get a nominal baud rate of 1 Mbps using the following settings

I am able to operate correctly at 2.5 Mbps using the setting below.

I am trying to get a data baud rate of 5 Mbps by setting the data rate prescaler to 0 above. However, I do not see any message transmission attempts on the bus (using a scope to watch the CANH/CANL pins) if I make that change. I also tried changing the MCAN clock prescalar to do so but to no avail.
Can somebody please verify if I am using valid settings ?