Part Number: TMS320F28030
Tool/software:
In our motor control inverter equipped with a TI microcontroller: TMS320F28030 and an NXP CAN transceiver,
when bus-off occurs, a high voltage not seen during normal operation occurs in the CAN differential voltage.
(The CAN-H/CAN-L potential difference is about 1.7V, but sometimes it appears as 1.7V + 0.6V = 2.3V,
as if noise is riding on the 1.7V potential on the H side.)
If you know the cause of this phenomenon, or if a similar phenomenon has occurred in the past, please let me know.
It is possible that a non-standard node with a baud rate slightly outside the MCU's allowable error range is connected, but is there any relationship between this and the current phenomenon?