Part Number: TMS320F28030
Tool/software:
The microcontroller (MS320F28030) and external oscillator are behaving abnormally,and CAN communication is abnormal.
The output amplitude of the external oscillator is becoming smaller due to heat.
Based on these facts, the following assumption is made, but is it correct?
If the output amplitude of the external oscillator simply becomes smaller,
there is no fluctuation in the input frequency, so no abnormality occurs in CAN communication.
If the output amplitude repeatedly increases and decreases, the number of inputs will fluctuate,
causing bit shifts in CAN communication and error frames.
If there are many error frames, the "Bus-off" state will occur.
When an oscilloscope is connected to obtain the raw waveform of the
external oscillator, the signal form changes and it cannot be measured.