Tool/software:
This is about the amplitude of the crystal oscillator input to the microcontroller.
I understand that it is better to have a low amplitude for the input signal, but I would like to confirm the following additionally.
- Is there a possibility of misjudgment if the amplitude is so low that it falls below the microcontroller's threshold level?
- If the amplitude is not constant and fluctuates up and down due to some influence, will the internal clock period fluctuate, resulting in an error frame in CAN communication?