This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: Watchdog software reset not working in F280049C

Part Number: TMS320F280049C


Tool/software:

below mentioned example i was trying to do watchdog timer reset .watchdog reset is not happing in controller its going for estop of address 0x3fb02a

i have tried with interrupt method also as mention below image .but its staying in while  loop SysCtl_resetDevice function

how i can do the watch dog reset by both the methods .please support to solve this issue ..

Regards,

Subash

  • Hi Subhash,

    If you are running with RAM configuration please set the EMU_BOOT to EMU_BOOT_RAM and if running from Flash set the EMU_BOOT to EMU_BOOT_FLASH.

    If Watchdog triggers Xrsn your application doesnt know where to boot/start from again, if you set the appropriate boot mode you would see that the application runs over again and triggers XRSn in loop.

    Pro tip : Check the RESC register and you would see the WDRSn bit to check if Watchdog triggered reset or not

    Thanks.

    To select the EMU boot mode see below :