This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: Unable to receive the data while using TMS320F28335 as master and TMS320F28379D as slave during SPI communication.

Part Number: TMS320F28379D
Other Parts Discussed in Thread: TMS320F28335,

Tool/software:

Hi All, 

I am using TMS320F28335 as master and TMS320F28379D as slave in SPI communication. Initially, I did run the example loop back with an interrupt code on both controllers separately, and they did work fine. Later, I adjusted code in TMS28335 to just transmit data and TMS28379D to receive data.  The edited codes for master and slave are given below. 

Master: 

//
// Included Files
//
#include "DSP28x_Project.h"     // Device Headerfile and Examples Include File

//
// Function Prototypes
//
//__interrupt void ISRTimer2(void);
__interrupt void spiTxFifoIsr(void);
void delay_loop(void);
void spi_fifo_init(void);
void error();

//
// Globals
//
Uint16 sdata;     // Send data buffer


//
// Keep track of where we are in the data stream to check received data
//
Uint16 rdata_point;

//
// Main
//
void main(void)
{
    Uint16 i;

    //
    // Step 1. Initialize System Control:
    // PLL, WatchDog, enable Peripheral Clocks
    // This example function is found in the DSP2833x_SysCtrl.c file.
    //
    InitSysCtrl();

    //
    // Step 2. Initialize GPIO:
    // This example function is found in the DSP2833x_Gpio.c file and
    // illustrates how to set the GPIO to it's default state.
    //
    // InitGpio();  // Skipped for this example
    
    //
    // Setup only the GP I/O only for SPI-A functionality
    //
    InitSpiaGpio();

    //
    // Step 3. Initialize PIE vector table:
    // Disable and clear all CPU interrupts
    ///
    DINT;
    IER = 0x0000;
    IFR = 0x0000;

    //
    // Initialize PIE control registers to their default state:
    // This function is found in the DSP2833x_PieCtrl.c file.
    //
    InitPieCtrl();

    //
    // Initialize the PIE vector table with pointers to the shell Interrupt
    // Service Routines (ISR).
    // This will populate the entire table, even if the interrupt
    // is not used in this example.  This is useful for debug purposes.
    // The shell ISR routines are found in DSP2833x_DefaultIsr.c.
    // This function is found in DSP2833x_PieVect.c.
    //
    InitPieVectTable();

    //
    // Interrupts that are used in this example are re-mapped to
    // ISR functions found within this file.
    //
    EALLOW;	        // This is needed to write to EALLOW protected registers
//    PieVectTable.SPIRXINTA = &spiRxFifoIsr;
    PieVectTable.SPITXINTA = &spiTxFifoIsr;
    EDIS;   // This is needed to disable write to EALLOW protected registers

    //
    // Step 4. Initialize all the Device Peripherals:
    // This function is found in DSP2833x_InitPeripherals.c
    //
    // InitPeripherals(); // Not required for this example
    spi_fifo_init();	  // Initialize the SPI only

    //
    // Step 5. User specific code, enable interrupts:
    //

    //
    // Initialize the send data buffer
    //
//    for(i=0; i<16; i++)
//    {
//        sdata[i] = i;
//    }
//    rdata_point = 0;

    //
    // Enable interrupts required for this example
    //
    PieCtrlRegs.PIECTRL.bit.ENPIE = 1;   // Enable the PIE block
    PieCtrlRegs.PIEIER6.bit.INTx1=1;     // Enable PIE Group 6, INT 1
    PieCtrlRegs.PIEIER6.bit.INTx2=1;     // Enable PIE Group 6, INT 2
    IER=0x20;                            // Enable CPU INT6
    EINT;                                // Enable Global Interrupts

    //
    // Step 6. IDLE loop. Just sit and loop forever (optional)
    //
    for(;;);
}

//
// Some Useful local functions
//

//
// delay_loop -
//
void 
delay_loop()
{
    long      i;
    for (i = 0; i < 1000000; i++)
    {
        
    }
}

//
// error -
//
void 
error(void)
{
    __asm("     ESTOP0");	          //Test failed!! Stop!
    for (;;);
}

//
// spi_fifo_init - 
//
void 
spi_fifo_init()
{
    //
    // Initialize SPI FIFO registers
    //
    SpiaRegs.SPICCR.bit.SPISWRESET=0; // Step 1: Reset SPI

    SpiaRegs.SPICCR.all=0x002F; // 16-bit character, Looping is disabled
    SpiaRegs.SPICTL.all=0x0006; // Interrupt dis-abled, Master/Slave XMIT enable0
    SpiaRegs.SPISTS.all=0x0000;  // Clearing SPI flags (OVERRUN_FLAG, INT_FLAG).
    SpiaRegs.SPIBRR=0x004A;     // Baud rate

    SpiaRegs.SPIFFTX.all=0xE068;       // Previous: C021 Enable FIFO's, set TX FIFO level to 8
//    SpiaRegs.SPIFFRX.all=0x6068;       // Set RX FIFO level to 8
    SpiaRegs.SPIFFCT.all=0x00;
    SpiaRegs.SPIPRI.all=0x0010;     // Set FREE bit: Halting on a breakpoint will not halt the SPI


    SpiaRegs.SPICCR.bit.SPISWRESET=1;  // Enable SPI

//    SpiaRegs.SPIFFTX.bit.TXFIFO=1;
//    SpiaRegs.SPIFFRX.bit.RXFIFORESET=1;
}

//
// spiTxFifoIsr -
//
__interrupt void 
spiTxFifoIsr(void)
{
    Uint16 i;
//    for(i=0;i<16;i++)
//    {
//       SpiaRegs.SPITXBUF=sdata[i];      // Send data
//    }
//
//    for(i=0;i<16;i++)                    // Increment data for next cycle
//    {
//        sdata[i] = sdata[i]+ 1;
//    }
    sdata  = 8;
    SpiaRegs.SPITXBUF=sdata;
    SpiaRegs.SPIFFTX.bit.TXFFINTCLR=1;  // Clear Interrupt flag
    PieCtrlRegs.PIEACK.all|=0x20;  		// Issue PIE ACK
}

////
//// spiRxFifoIsr -
////
//__interrupt void
//spiRxFifoIsr(void)
//{
//    Uint16 i;
//    for(i=0;i<8;i++)
//    {
//        rdata[i]=SpiaRegs.SPIRXBUF;		// Read data
//    }
//
//    for(i=0;i<8;i++)                    // Check received data
//    {
//        if(rdata[i] != rdata_point+i)
//        {
//            error();
//        }
//    }
//    rdata_point++;
//    SpiaRegs.SPIFFRX.bit.RXFFOVFCLR=1;  // Clear Overflow flag
//    SpiaRegs.SPIFFRX.bit.RXFFINTCLR=1; 	// Clear Interrupt flag
//    PieCtrlRegs.PIEACK.all|=0x20;       // Issue PIE ack
//}

//
// End of File
//

Slave : 

//
// Included Files
//
#include "F28x_Project.h"

//
// Globals
//
Uint16 sdata[2];     // Send data buffer
Uint16 rdata;     // Receive data buffer
Uint16 rdata_point;  // Keep track of where we are
                     // in the data stream to check received data
Uint16 i;

//
// Function Prototypes
//
interrupt void spiTxFifoIsr(void);
interrupt void spiRxFifoIsr(void);
void delay_loop(void);
void spi_fifo_init(void);
void error();

//
// Main
//
void main(void)
{


//
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the F2837xD_SysCtrl.c file.
//
   InitSysCtrl();

//
// Step 2. Initialize GPIO:
// This example function is found in the F2837xD_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
// Setup only the GP I/O only for SPI-A functionality
//
   InitSpiaGpio();

   //
   // Step 4. Initialize the Device Peripherals:
   //
      spi_fifo_init();   // Initialize the SPI only
//
// Step 3. Initialize PIE vector table:
// Disable and clear all CPU interrupts
//
   DINT;
   IER = 0x0000;
   IFR = 0x0000;

//
// Initialize PIE control registers to their default state:
// This function is found in the F2837xD_PieCtrl.c file.
//
   InitPieCtrl();

//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example.  This is useful for debug purposes.
// The shell ISR routines are found in F2837xD_DefaultIsr.c.
// This function is found in F2837xD_PieVect.c.
//
   InitPieVectTable();

//
// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
//
   EALLOW;  // This is needed to write to EALLOW protected registers
   PieVectTable.SPIA_RX_INT = &spiRxFifoIsr;
//   PieVectTable.SPIA_TX_INT = &spiTxFifoIsr;
   EDIS;    // This is needed to disable write to EALLOW protected registers



//
// Step 5. User specific code, enable interrupts:
//

////
//// Initialize the send data buffer
////
//   for(i=0; i<2; i++)
//   {
//      sdata[i] = i;
//   }
   rdata_point = 0;

//
// Enable interrupts required for this example
//


//   IER = 0x20;                              // Enable CPU INT6 (SPI interrupt group)
//   PieCtrlRegs.PIEIER6.bit.INTx2 = 1;       // Enable PIE Group 6, INT 2 (SPI RX)


   PieCtrlRegs.PIECTRL.bit.ENPIE = 1;     // Enable the PIE block
//   PieCtrlRegs.PIEIER6.bit.INTx1 = 1;     // Enable PIE Group 6, INT 1
   PieCtrlRegs.PIEIER6.bit.INTx2 = 1;     // Enable PIE Group 6, INT 2
   IER |= M_INT6;                         // Enable INT6 in CPU;                              // Enable CPU INT6
   EINT;                                  // Enable Global Interrupts

//
// Step 6. IDLE loop. Just sit and loop forever (optional):
//
    for(;;);
}

//
// delay_loop - Function to provide delay
//
void delay_loop()
{
    long i;
    for (i = 0; i < 1000000; i++) {}
}

//
// error - Function to halt debugger on error
//
void error(void)
{
    asm("     ESTOP0");  //Test failed!! Stop!
    for (;;);
}

//
// spi_fifo_init - Initialize SPI FIFO
//
void spi_fifo_init()
{
    //------ Modified code ------------------------
    //
    // Initialize SPI FIFO registers
    //
    SpiaRegs.SPICCR.bit.SPISWRESET=0; // Step 1: Reset SPI

    SpiaRegs.SPICCR.all=0x002F; // 16-bit character, Looping is disabled
    SpiaRegs.SPICTL.all=0x0000; // Interrupt dis-abled, Master/Slave XMIT enable0
    SpiaRegs.SPISTS.all=0x0000;  // Clearing SPI flags (OVERRUN_FLAG, INT_FLAG).
    SpiaRegs.SPIBRR.bit.SPI_BIT_RATE = 99;     // Baud rate

    SpiaRegs.SPIFFTX.all=0xE068;       // Previous: C021 Enable FIFO's, set TX FIFO level to 8
//    SpiaRegs.SPIFFTX.bit.SPIFFENA = 1;   // FIFO enhancement mode ON
    SpiaRegs.SPIFFRX.all=0x6069;         // Set RX FIFO level to 8
    SpiaRegs.SPIFFCT.all=0x00;
    SpiaRegs.SPIPRI.all=0x0010;          // Set FREE bit: Halting on a breakpoint will not halt the SPI


    SpiaRegs.SPICCR.bit.SPISWRESET=1;  // Enable SPI

//    //------ Below code is original code ------------------------
//    //
//    // Initialize SPI FIFO registers
//    //
//    SpiaRegs.SPIFFTX.all = 0xC028;    // Enable FIFOs, set TX FIFO level to 8
//    SpiaRegs.SPIFFRX.all = 0x0028;    // Set RX FIFO level to 8
//    SpiaRegs.SPIFFCT.all = 0x00;
//
    SpiaRegs.SPIFFTX.bit.TXFIFO=1;
    SpiaRegs.SPIFFRX.bit.RXFIFORESET=1;
//
////    //
////    // Initialize core SPI registers
////    //
//    InitSpi();

}

////
//// spiTxFifoIsr - ISR for SPI transmit FIFO
////
//interrupt void spiTxFifoIsr(void)
//{
//    Uint16 i;
//    for(i=0;i<2;i++)
//    {
//       SpiaRegs.SPITXBUF=sdata[i];      // Send data
//    }
//
//    for(i=0;i<2;i++)                    // Increment data for next cycle
//    {
//       sdata[i] = sdata[i] + 1;
//    }
//
//    SpiaRegs.SPIFFTX.bit.TXFFINTCLR=1;  // Clear Interrupt flag
//    PieCtrlRegs.PIEACK.all|=0x20;       // Issue PIE ACK
//}

//
// spiRxFifoIsr - ISR for SPI receive FIFO
//

interrupt void spiRxFifoIsr(void)
{
//    Uint16 i;
//
//    for(i=0; i<8; i++)
//    {
//        rdata[i]=SpiaRegs.SPIRXBUF;     // Read data
//    }

    rdata = SpiaRegs.SPIRXBUF;     // Read data


//    for(i=0; i<2; i++)                  // Check received data
//    {
//        if(rdata[i] != rdata_point+i)
//        {
//            error();
//        }
//    }

//    rdata_point++;

    SpiaRegs.SPIFFRX.bit.RXFFOVFCLR=1;  // Clear Overflow flag
    SpiaRegs.SPIFFRX.bit.RXFFINTCLR=1;  // Clear Interrupt flag
    PieCtrlRegs.PIEACK.all|=0x20;       // Issue PIE ack
}

//
// End of file
//

The problem here is that Master is able to transmit the data. which I cross-checked by measuring signals across CLK, SIMO pins, and the slave select line. but slave is unable to receive data. Could you please let me know if I am doing anything wrong in modifying code or anything else I have to change?

  • Hi Kranthi,

    If you are in master mode, transmitting data, and immediately attempting to read from the receive buffer, you may be reading corrupted data because you are reading too quickly and only part of the data has been received. Ensure the transmit FIFO level has space available before writing to TXBUF to transmit data. Inversely, check that the receive FIFO level to has the proper amount of complete and valid data characters received into RXBUF before reading from RXBUF.

    Please only provide relevant code with any comments removed.

    Best Regards,

    Aishwarya

  • Hi Aishwarya,

    I was initially facing issues because I hadn’t enabled the TX FIFO reset, but fortunately, I managed to troubleshoot all the code-related problems. However, I’ve encountered a new issue now. I have connected three TMS320F28379D slave controllers to a TMS320F28335 master, and I am transmitting sinusoidal signals from the master to the three slaves. The waveforms captured using the graph window in CCS are shown below.

     Fig.1

    The master generates the above waveform and transmits it to the slaves. While Slave 1 is receiving this signal, the slave select lines for Slaves 2 and 3 are kept high. I am using this approach to transmit the signal to all three slaves individually.

    The data received on slave 1 (slave 1 is connected to a PC) is shown below, and everything looks perfect.

    Fig. 2

    However, data received on slave 2 (slave 2 is connected to a laptop) has glitches, as shown below.

     Fig.3

    I connected Slave 1 to a laptop and Slave 2 to a PC, but I still noticed glitches in Slave 1. Could this be related to the USB version of the laptop? Also, the glitches seem to worsen when the laptop is plugged into the charger. I am using a 25 MHz SPI clock frequency. Any idea why this is happening?

  • Kranthi,

    Happy to hear that. It sounds like the SPI communication itself is working fine, but some graph has glitches. Refer to this guide to debug the Graph Tool: 7.7. Graph Tools — Code Composer Studio 12.8.0 Documentation

    Best Regards,

    Aishwarya

  • Hello Aishwarya ji,

    I went through the graph tools and verified that all parameters were set correctly, but the glitches persisted. Finally, I decided to change the power supply source for the TMS320F28379D slaves connected to the laptops, and everything is working perfectly now.

  • Kranthi,

    Thanks for the update. If you do not have any other questions, please mark this thread as closed. 

    Best Regards,

    Aishwarya