This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
"On future C2000 devices, there will be the capability to have more than two CMPx values so that you can generate multiple pulses at different duty cycles within a single EPWM period, without needing to use the dead-band module or up-down count mode."
Is this feature available now on the C2000 devices?
I need to generated two pulses within a single EPWM period. Is it possible to do on 28379D device?
It is in relation to the comment on thread here -
e2e.ti.com/.../tms320f280049c-configuration-of-the-epwm-module-to-achieve-the-desired-pwm-waveform
Apoorv,
It is not possible on F28379D device as per the method you described. Not even using F28379D device. It can be done using CLB as shown in e2e post you sent.
Regards,
Sumit