This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi!
I'm trying to use the SCI and I've started with Example_2806xSci_Echoback.c. I have a docking station and the controlcard with F28069. I use only the USB connection. I start Hyperterminal, load the program, connect with hyperterminal and then start the program from code composer debug window. Can this work? I mean with only one connection.
I've checked in Device manager and there is Texas Instruments XDS100+RS232 V1.0 on COM17. I suppose this is the COM port I must set in hyperterminal. Code composer is using the same port I guess.
Anyway, I don't receive the message 'Hello world' nor the next ones. Is there a hardware jumper that I must set or something else?
Thank you,
Monica
Hi!
Was some time ago, but I remeber I was able to read some characters in Hyperterminal and send characters to Piccolo.
If you are using a development board (I use TMDXDOCK28069) check the jumpers of the Tx and Rx lines. On TMDXDOCK28069 J9 must be connected (Rx line).
Monica