Tool/software:
Hello,
Section 3.15.8.1 of SPRUI33H defines the values that should be seen in the PARTIDL register. But when I access this part thru CCS Memory Browser I get a value that does not agree with the manual. Specifically the high byte of PARTIDL is defined to read as 0x00 while in the memory browser I see 0x20. I can mask this bit during my routine to determine which processor (F280041x or F280049x) is in use but worry there might be other bits that could read different than the manual so wanted to get clarification on why the difference exists.
Thanks - Bruce