Part Number: TMS320F28P650DK
Tool/software:
Hi Champ,
I am reconfirming for my customer.
It is noted that it leaves 8W length (0x25FF8-0x25FFF) in the end of LS9, those memory can't be used by CPU1.
If user configures LS8 & LS9 as CLA program in .cmd file as below,
RAMLS_CLA_PROG : origin = 0x004000, length = 0x004000 // LS8~LS9 for CLA_PROGRAM
(1). Would the errata also affect the CLA core for using the last 8W length of LS9 as CLA program ? Should be NOT, right ?
In this post, may I reconfirm the conclusion is that user can't assign LS0, LS1, LS8 and LS9 RAM as CLA program memory as a combined memory sector shown as below, right ?
RAMLS_CLA_PROG : origin = 0x004000, length = 0x005000 // LS8~LS9~LS0~LS1 for CLA_PROGRAM
(3). Following #2, if LS8 & LS9 & LS0 & LS1 could be assigned as CLA program, in this scenario, should 8W length on LS9 be reserved to avoid this errata ?
Thanks and regards,
Johnny