Hi,
BACKGROUND
I am running
C:\TI\controlSUITE\development_kits\HVMotorCtrl+PfcKit_v1.6\HVPM_Sensorless_2833x\HVPM_Sensorless.c
on a eZdsp 28335 platform using CSv4
I have the following problem with the PWM output (I've been using build level 1 and 2)
PROBLEM
Setting VDtesting 0.5 (beautiful 3 phase space vector switching pattern 120 degrees phase seperation- observed via low pass filter RC)
Setting VDtesting to 0 (I would expect the PWM to be OFF - no demand). however I see a slow triangular waveform on all 3 phases (all in phase). It's period is 1.3seconds and its magnitude is 1.25V (on a 5V rail).
When Viewing the PWM output with VdTesting =0.5, with a longer time base the whole switching waveform is mapped onto this slow 1.3s carrier wave.
NOTE
I'm running the PWM with a base of 5kHz instead of 10kHz.
....
Answer would make my Christmas...probably my year.
Thanks.