Part Number: TMS320F28388D
Dear Team,
I have a question regarding the ePWM module and more specifically the Dead-Band Generator submodule.
What is the expected behavior of the deadband submodule when the ePWM is setup in up-down count mode, active high complementary signal pairs output, and the selected CMPA value is too close to 0 or PRD such that the following conditions are met (CMPA < Deadband/2) or (CMPA > PRD – (Deadband)/2)?
The following excerpt from the ‘spruii0f’ reference manual describes that the actions specified by the AQCTL register do not take effect. To avoid this behavior, it suggests setting both the CAU and CAD to the same behavior (both set or both clear):
From our testing, it appears that when (CMPA < Deadband/2) or (CMPA > PRD – (Deadband)/2) the AQCTL register is still in effect due to the complementary side being implemented but the impacted side stays low. This seems to conflict with the AQCTL register being ignored.
Examples:
Please let us know if you have any questions.
Thank you,
Daniel Waleniak