Other Parts Discussed in Thread: TMS320F2812
Hello to everyone,
I am new to this DSP board and would like to ask for some help in troubleshooting, ie. to connect to my PC.
Below are some of the technical information
Operating System: Windows XP 32bit
DSP: TMS320F2812
Software: CCS 3.1
Drivers: C2000 -> CCS 3.1 Driver Release 3.01.04C
Error Message when I tried connecting in CCS 3.1:
Error connecting to the target: Error 0x80000200/-1031 Fatal Error during: OCS, Device driver: Problem with the Emulation Controller. It is recommended to RESET EMULATOR. This will disconnect each target from the emulator. The targets should then be power cycled or hard reset followed by an emureset and reconnect to each target. Sequence ID: 0 Error Code: -1031 Error Class: 0x80000200 I/O Port = 378 Board Name: F2812 eZdsp Cpu Name: cpu_0 Abort: Close Code Composer Studio. Retry: Try to connect to the target again. Cancel: Remain disconnected from the target Diagnostic: Run diagnostic utility.
Additional Information: I have tried to reset the emulator using the SDConfig program. And SDConfig replied affirmatively to my reset command. In my CCS Setup, I have chosen
F2812 eZdsp. Below is my SD Config screenshot.
Please advise.
Let me know if more information is needed. Thank you for reading.
Have a nice day.