Part Number: TMS320F28379D
Other Parts Discussed in Thread: TMS320F28377D, TPS62420, TPS3702
Hello there,
I am currently using the 176-Pin TMS320F28377D in a design and have been experiencing catastrophic microcontroller failures during power-up of the circuit card assembly. These failures occur intermittently, about one-third of the time.
I suspect that it may be related to the power supply topology I am using for VDDIO and VDD. My current configuration uses a cascading power architecture, where a 3.3 V buck regulator (VDDIO) feeds a second 1.2 V buck regulator (VDD). Because of this arrangement, there is a delay between the power-up of the two supply rails, ~2ms. The microcontroller is held in reset until the PGood of the regulators is high.
I am meeting the power sequencing requirements outlined in Section 6.9.1.2 and ensuring that VDD does not exceed VDDIO by more than 0.3 V. However, VDDOSC and VDD are not powering up at the same time.
Could this delay in the power sequencing, or the fact that VDDOSC and VDD are not powering up simultaneously, be contributing to the intermittent failures? I've attached a couple of rise time capture between the 3.3 V and 1.2 V regulators. I would appreciate any insight into whether my current power topology or sequencing approach could be causing this issue.