Other Parts Discussed in Thread: CONTROLSUITE
Hi all.
I'm using simulink to generate C code for the c2000 mcu and I would like to add flash-based eeprom emultaion features using the flash API provided by texas instruments.
Running the flash API example using CCSv5 to build theproject, all works fine, but when I try to build the simulink model that uses flash API functions I get alinker error:
undefined first referenced
symbol in file
--------- ----------------
_Flash28_API_LoadEnd ./derived/flashAPItest_main.obj
_Flash28_API_LoadStart ./derived/flashAPItest_main.obj
_Flash28_API_RunStart ./derived/flashAPItest_main.obj
It seems like the linker is unable to find the symbols listed above, which are defined in the "Flash28335_API_V210.lib" file. I added the path to the directory containing the .lib file (C:\ti\controlSUITE\libs\utilities\flash_api\2833x\28335\v210\lib\) among the "Include directories" list in the custom code section of the code generation menu and I also added the filename to the " libraries" list, so I think the linker should be able to link the file...
Any suggestions?
Thanks in advance