Other Parts Discussed in Thread: CCSTUDIO
I have a custom F28335 based board to which I connect using the Spectrum Digital XDS510LC JTAG emulator. Previously, I have been using an ezdsp board (also F28335) on the same computer - but I do not anymore.
Occasionally, CCS Setup "forgets" about my custom board and the ezdsp board reappears in "My System". I have to remove the ezdsp board and re-add the "F28335 XDS510USB Emulator" board. (Just to clarify, i DO NOT want ezdsp board to be there at all. It gets added automagically each time this happens.)
- This happens when something goes wrong, i.e. a CCS- or emulator-crash (too often, creating irritation)
- I believe it didn't happen before I switched to running from FLASH (using programmer plug-in)
- Same issue spotted on another computer
Any ideas, solutions, similar experiences?
CCS 3.3.80.11, BIOS 5.32, CGTs 5.0.2