Hi Champs,
one of my customer is developing with PiccoloA TMS320F28027 and is using PWM as descirbed in doc. SPRUGE9. They need to use the two PWM independently (through AQCSFRC), and in order to do this they are trying to set CSFB and CSFA independently. The resul is that the two PWM seem to work in complimentary mode instead of the independent mode. What should be the bug in code?
Thanks and regards,
Alberto