Hi there,
i was trying to use the PWM8B output on GPIO15 and i can see that the output is not present on this PIN.
Is this a problem of the F28M36 control card, or is the DSP core that has an issue with this pin?
I have already tried with 3 simiar boards, is the same. The GPIO setup should be ok, as in the example, and i give rights from the M3 master core. PWM8A is working on GPIO14, pin 62, and PWM8B is working on GPIO61, pin 126 but not on GPIO15 pin 64.
Has anyone experienced the same issue on this matter?
Best regards,
Ionut