This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I bought a TMDSDC3359 Data Concentrator Evaluation kit, together with 2 tmdsplckitV3 nodes.
I got it up and running, I can register the 2 nodes on the prime base node. I did also manage to get IEC 61334 to register and communicate. But it appears that there is no IPv4 support on the Prime Base node. The documentation is scares, and difficult to find.
The software and documentation (PRIME Data Concentrator Software and Documentation) on the http://www.ti.com/tool/TMDSDC3359 page isn't for the TMDSDC3359. It is for the tmdsplckitV3 kit.
I need to know how to setup a IPv4 connection to the base node. I implemented a packet sniffer on another node, and the best I can see is that TI didn't implement the IPv4 or IPv6 as per the PRIME 1.3.6 specification. All the messages are ignored. and after confirming it by hand, they are valid and should be responded to by the base node, even if to deny the request.
All their software also seems to be for the PHY interface, and not the PRIME interface. Is there a document that describes how to setup a IPv4 connection over the PRIME.
Regards,
Riaan Oosthuizen