Other Parts Discussed in Thread: TMS320F2812
Hi,
Iam making a custom flash programming tool to re-program my TMS320F2812 flash module in SCI-A boot mode.
Issue:
I noticed when sending data over rs232 to bootloader that bootloader does not respond/acknowledge received data and no error messages are sent at all.
I'm using the provided test program to test comm is ok but the line is too quiet i think. There is no way to know whether data has been received on the bootloader side.
I've looked through the spru095c.pdf and there is no information about bootloader response messages/errors at all.
Am i missing something?
thanks
serge
Test Program as sent to bootloader:
Note: used Comport toolkit to send 2 bytes at a time (e.g. "10 AA")
10 AA ; 0x10AA 16-bit key value
00 00 ; 8 reserved words
00 00
00 00
00 00
00 00
00 00
00 00
00 00
00 3F ; 0x003F8000 EntryAddr, starting point after boot load completes
80 00
00 05 ; 0x0005 − First block consists of 5 16-bit words
00 3F ; 0x003F9010 − First block will be loaded starting at 0x3F9010
90 10
00 01 ; Data loaded = 0x0001 0x0002 0x0003 0x0004 0x0005
00 02
00 03
00 04
00 05
00 02 ; 0x0002 − 2nd block consists of 2 16-bit words
00 3F ; 0x003F8000 − 2nd block will be loaded starting at 0x3F8000
80 00
77 00 ; Data loaded = 0x7700 0x7625
76 25
00 00 ; 0x0000 − Size of 0 indicates end of data stream