This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am using SCI FIFO (4 level) to transfer chunk of data (currently in loopback mode to test the driver).
Issue:
1. I find first byte is always missed which is send from TX INTR. (If I send first byte as dummy data and then load FIFO with correct 4 bytes, then all is received correctly.)
This is not mentioned in FIFO operation section of controller manual literature.
Whereas in document SCI-A_Tech Ref Manual I find section 1.1.5.3 (Wake-Up Temporary Flag) which talks about first byte being ignored in case of block transfer.
Conclusion: So, all the time I need to send 5 Bytes instead of 4 bytes in case of FIFO operation to work properly.
Can someone confirm my understanding?
Hi Gautam,
thanks for quick reply. below are configuration values. Which seems to be OK as per manual:
SciaRegs.SCICCR.all = 0x0007;
SciaRegs.SCICCR.bit.LOOPBKENA = 1;
SciaRegs.SCICTL2.bit.TXINTENA = 1;
SciaRegs.SCICTL2.bit.RXBKINTENA = 1;
SciaRegs.SCIHBAUD = 0x0000;
SciaRegs.SCILBAUD = SCI_PRD;
SciaRegs.SCIFFTX.all = 0xE020;// E090 //0xC022; think to clr bit 6 also later
SciaRegs.SCIFFRX.all = 0x2034; //0x2034; //0x0022;
SciaRegs.SCIFFCT.all = 0x00;
SciaRegs.SCICTL1.all = 0x0023;
Does the sample code "Example_2806xScia_FFDLB.c" work for you or it too behaves the same way?
Gautam,
This example has worked well for me in past, and I have retained most of its configuration other than FIFO water levels and interrupt settings.
this example is not interrupt based. I receive RX interrupt after 4 bytes are received in FIFO buffer. Somehow, the first byte is not getting pushed into FIFO and getting discarded.
==> In my first post, I have mentioned about reference manual section where this behavior is OK during multiprocessor communication mode.
I wanted to know, if it is OK for normal multibyte transfer mode also OR I am missing some settings.. (I have pushed all settings in previous post which are used by me)
Guys,
it worked now. Issue was with SCI configuration register settings for FFTX and FFRX.