Hi,
I am using Delfino F28377 for my Motor control. I am trying to implement current control in CLA. I am getting CLA program memory is insufficient. Presently I configured LS5 as program RAM, and as per manual, i can assign any LSx memory block as program. Is it possible to use both LS4 and LS5 for program. If so, how to write in the *.cmd file. can I just write
Cla1Prog : > RAMLS5 | RAMLS4, PAGE=0
and write necessary value in the register.
MemCfgRegs.LSxMSEL.bit.MSEL_LS5 = 1;
MemCfgRegs.LSxCLAPGM.bit.CLAPGM_LS5 = 1;
MemCfgRegs.LSxMSEL.bit.MSEL_LS4 = 1;
MemCfgRegs.LSxCLAPGM.bit.CLAPGM_LS4 = 1;
Also I want to know can I use GS0 block for .ebss. As present block LS2 for .ebss is not sufficient for my code.
Thanks & Regards,
Rathinavel