Hello.
I have just bought a three phase BLDS/PMSM motor kit with DRV8301 and the C2000 Piccolo F28035 MCU controlCARD. I have tried my motor in the preflashed GUI, and it spins perfectly.
I have now started to program in CCS, and I see that there are several labs that takes me through the process of identifying and spinning my motor. But, my problem is that the labs looks like they are specified for the F2802xF, F2805xF and F2806xF. I have the F28035, and wonder if I can use the same labs for my MCU?
Can anyone help me with this? Is it possible to run these laba on my F28035 MCU? If not, is there any other available labs? And if, why do I get the error above?
Edit:
I have found out that there are two labs that are designed for the F28035 located in the ControlSuite folder. But these isn't as good as the labs in the motorware-folder (labs 01 to 13e).
Are there anyone that knows how to make the "good" labs work with the F28035.
Thanks!