Hello,
I am using the f28335 delfino board and accidentally while working on a sensor ,the sensor short circuited and because of this the 3.3V and ground on the docking station got shorted.After this the U1 and U2 IC on the docking station is getting heated up and also the right side of the control card(as seen in pic) is also getting heated up.
Also when i connect it to PC it says USB cannot be recognized and in CCS says it cannot connect to target.
what procedure can i follow to get it working again or should i replace the entire setup ?