This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi everyone,
I would like to make the code connect from DSP TMS320F28335 to IC bq76940 (TI), family of robust analog front-end (AFE). I see that they can communicate by I2C communication.
Is that possible? And can I get the support from TI to make the code?
Thank you very much!
Hi Gautam,
I am making the code and I get problem with I2C signal.
When the DSP is not connect to the BQ76940, the I2C signal which is measured at DSP is good, like this
The IC is other PCB, and when I connect DSP to IC by some line, the frequency is change to 84 khz of SCL and SCL signal is distorted, like this:
With the SCL signal like that, is there any problem for DSP to understand the news is transfer from the BQ76940?
And from the I2C signal, how I can determine the cell voltage (the Lithium cell are connect to IC, IC measure the cell voltage and report to DSP)
Thank and Best regards,