This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello
I'm implementing EtherCAT on DSP, with following setting:
I'm having a problem when using malloc() to get some memory space for receiving data. When my program execute malloc(128), it will fall into ILLEGAL_ISR.
I think I give enough size to .esysmem. How can I fix this problem?
Following is how my linker being set
MEMORY { PAGE 0 : /* BEGIN is used for the "boot to SARAM" bootloader mode */ /* BOOT_RSVD is used by the boot ROM for stack. */ /* This section is only reserved to keep the BOOT ROM from */ /* corrupting this area during the debug process */ BEGIN : origin = 0x000000, length = 0x000002 /* Boot to M0 will go here */ BOOT_RSVD : origin = 0x000002, length = 0x00004E /* Part of M0, BOOT rom will use this for stack */ RAMM0 : origin = 0x000050, length = 0x0003B0 RAML0 : origin = 0x008000, length = 0x001000 RAML1 : origin = 0x009000, length = 0x004000 //please aware the mapping overlap between PAGE0 and PAGE1 ZONE7A : origin = 0x200000, length = 0x00FC00 /* XINTF zone 7 - program space */ CSM_RSVD : origin = 0x33FF80, length = 0x000076 /* Part of FLASHA. Program with all 0x0000 when CSM is in use. */ CSM_PWL : origin = 0x33FFF8, length = 0x000008 /* Part of FLASHA. CSM password locations in FLASHA */ ADC_CAL : origin = 0x380080, length = 0x000009 RESET : origin = 0x3FFFC0, length = 0x000002 IQTABLES : origin = 0x3FE000, length = 0x000b50 IQTABLES2 : origin = 0x3FEB50, length = 0x00008c FPUTABLES : origin = 0x3FEBDC, length = 0x0006A0 BOOTROM : origin = 0x3FF27C, length = 0x000D44 PAGE 1 : RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */ RAML4 : origin = 0x00D000, length = 0x000C00 RAML5 : origin = 0x00DC00, length = 0x000C00 RAML6 : origin = 0x00E800, length = 0x000C00 RAML7 : origin = 0x00F400, length = 0x000C00 ZONE7B : origin = 0x20FC00, length = 0x000400 /* XINTF zone 7 - data space */ } SECTIONS { /* Setup for "boot to SARAM" mode: The codestart section (found in DSP28_CodeStartBranch.asm) re-directs execution to the start of user code. */ codestart : > BEGIN, PAGE = 0 ramfuncs : > RAML0, PAGE = 0 .text : > RAML1, PAGE = 0 .cinit : > RAML0, PAGE = 0 .pinit : > RAML0, PAGE = 0 .switch : > RAML0, PAGE = 0 xintffuncs : LOAD = RAML1, RUN = ZONE7A, LOAD_START(_XintffuncsLoadStart), LOAD_END(_XintffuncsLoadEnd), RUN_START(_XintffuncsRunStart), PAGE = 0 .stack : > RAMM1, PAGE = 1 .ebss : > RAML4, PAGE = 1 .econst : > RAML5, PAGE = 1 .esysmem : > RAMM1, PAGE = 1 IQmath : > RAML1, PAGE = 0 IQmathTables : > IQTABLES, PAGE = 0, TYPE = NOLOAD IQmathTables2 : > IQTABLES2, PAGE = 0, TYPE = NOLOAD FPUmathTables : > FPUTABLES, PAGE = 0, TYPE = NOLOAD DMARAML4 : > RAML4, PAGE = 1 DMARAML5 : > RAML5, PAGE = 1 DMARAML6 : > RAML6, PAGE = 1 DMARAML7 : > RAML7, PAGE = 1 ZONE7DATA : > ZONE7B, PAGE = 1 .reset : > RESET, PAGE = 0, TYPE = DSECT /* not used */ csm_rsvd : > CSM_RSVD PAGE = 0, TYPE = DSECT /* not used for SARAM examples */ csmpasswds : > CSM_PWL PAGE = 0, TYPE = DSECT /* not used for SARAM examples */ /* Allocate ADC_cal function (pre-programmed by factory into TI reserved memory) */ .adc_cal : load = ADC_CAL, PAGE = 0, TYPE = NOLOAD }
Your help would be much appreciated.
Thanks a lot
Yi-Lin
Thanks for replying
When I build my project, I will get a warning message:
warning: creating ".sysmem" section with default size of 0x400; use the -heap
option to change the default size.
And I meet an embarrassing problem that I can't open my CCS3.3 now.
When I open CCS, it will get stuck at the splash after long time waiting, the icon of CCStudio Monitor will gray out.
I installed the CCS on WinXP SP3 on VMware Player v6.0.4.
Is there any suggestion to fix this?
Thanks for replying
When I build my project, I will get a warning message:
warning: creating ".sysmem" section with default size of 0x400; use the -heap
option to change the default size.
And I meet an embarrassing problem that I can't open my CCS3.3 now.
When I open CCS, it will get stuck at the splash after long time waiting, the icon of CCStudio Monitor will gray out.
I installed the CCS on WinXP SP3 on VMware Player v6.0.4.
Is there any suggestion to fix this?
Hello Gautam
Thanks for your replying.
I succeed to open CCS by disconnecting my ICE(BH-USB-560v2) from my computer. Looks strange but it works...
As suggested by Christopher, the illegal_ISR problem is solved after I give more space to .esysmem.
PAGE 1 : RAMM1 : origin = 0x000400, length = 0x000400 /* on-chip RAM block M1 */ RAMM2 : origin = 0x00D000, length = 0x000B60 RAML4 : origin = 0x00DB60, length = 0x001000 RAML5 : origin = 0x00EB60, length = 0x001000 RAML6 : origin = 0x00FB60, length = 0x000250 RAML7 : origin = 0x00FDB0, length = 0x000250
And refer to
http://e2e.ti.com/support/microcontrollers/c2000/f/171/p/438147/1570672
I allocate same space for both .sysmem and .esysmem section
.esysmem : > RAMM1|RAMM2, PAGE = 1 .sysmem : > RAMM1|RAMM2, PAGE = 1
But the "creating ".sysmem" section with default size of 0x400;" warining still exist until I set a value to the Heap size in Build options.
Since there is no error or warning occur and program works fine, do I need to set the Heap size in Build options same as .sysmem?
Thanks a lot