This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Onur,
It looks like the ENC28J60 supports a standard SPI interface:
Note that the ENC28J60 will receive the SPICLK from the 28x therefore the 28x SPI will be configured fro MASTER mode. You can also use the 28x SPISTE signal for the ENC28J60 CS. For receiving the interrupt signal you may want to use one of the XINT pins.
As Gautum pointed out, the SPI example code is a good starting point.
Jeff