Hi,
I have a DRV8312-C2 Kit and I am running the motor that came with the Kit using DRV8312GUI_Main.c.
Can somebody tell me, how do i modify the code to get 100% duty cycle for the PWMxB signals (the signals fed to the RESET_X input of the DRV8312)? I posted a question regarding current waveform DRV8312 issue on Motor Driver Forum and was asked to modify the PWMxB signals.
Below are some other questions:
Looking at the BLDCPWM_Macro(),
1. what is the function of the variables Tmp and Tmp2?
2. What does half mean in EPwm1Regs.CMPA.half.CMPA = (int16)(Tmp>>15)?
Thanks!