This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hello,
now i could drive motor to 10rpm,and i didn't understand the parament define in detail.
1. excitation magnitude is in volts per unit
it means if i set it 1.0, the hardware will output a 1.0V on phase voltage?
and this parament must be use a current probe on phase to obtain the right value?
2.how could i confirm the IPD_HFI_LP_SPD_FILT_HZ and IPD_HFI_HP_SPD_FILT_HZ value?
is there any recommand ways or the "right direction" to figure out them.
now i just set them with 0.
3.wait time
is this parament only used in motor startup?
if i set it with 0.8(both coarse and fine),it will not have a bad affects on motor spin, right?
4.IqMaxLf and IqSlopeLf were easy to understand,but what freqHigh define?
does it take RPM as the unit? because of i found that no matter what value i set (freqHigh and freqLow), it always using the HFI angle and speed as input.