This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I try to use Experimenter's Kit - Piccolo F28069 with CCSV6 under Linux but I have got lot of errors during compilation indicating that it doesn't find specific header file while it really in the folder and folder include path declared correctly !
I check in the menu "project" " properties" and remarked that Experimenter's Kit - Piccolo F28069 doesn't appear in the selection menu, only Experimenter's Kit - Piccolo F28035. So I presume that dedicated libraries are loaded with and this is the reason why I got lot of errors...
Does somebody experimented it also ? Does somebody has got solution ?
Thanks for your answer,
Regards,
OL
Thanks for your answer Kyle,
Here under print screens of CCSV6 settings
Under Windows XP and 7 it works (CCSV6 version : 6.1.3.00033 and CCSV6 Linux Version: 6.1.0.00104 ) but under Linux Ubuntu 16.04 TLS ou 15.10 when I build the project, it performs (it seems) path errors such as :
Description Resource Path Location Type
bidule.c /xxxxx/Sources line 1 C/C++ Problem
F28069_Init.h xxxxx/Headers line 1 C/C++ Problem
Include_Project_Files.h xxxxx/Headers line 1 C/C++ Problem
Include_Project_Files.h xxxxxHeaders line 20 C/C++ Problem
expected a truc.c xxxxx/Sources line 1 C/C++ Problem
expected a truc1.c xxxxx/Sources line 1 C/C++ Problem
unrecognized truc2.c xxxxx/Sources line 1 C/C++ Problem
unrecognized token truc.c xxxxx/Sources line 1 C/C++ Problem
F2806x_DefaultISR.h xxxxx/Headers line 31 C/C++ Problem
However I have got the same project and the same folder tree, same settings so I've some difficulties to understood....
Please let me know if you already had these troubles.
Thank you for your help
OL
Solution found by adding :
sudo apt-get install libgcrypt11
sudo apt-get update
After that everything works perfectly !