This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8312-C2-KIT: Interface with F28069 Piccolo Experimenter Kit

Part Number: DRV8312-C2-KIT
Other Parts Discussed in Thread: MOTORWARE, DRV8312, C2000WARE-MOTORCONTROL-SDK

Hello,  

I have the DRV8312-C2-KIT as well as the F28069 Piccolo Experimenter Kit.  I bought the second kit in order to preform the 13 Labs in Motorware software package.  I know that the F28069 control card goes into the DRV8312 board, however there is no USB on the F28069 control card.  From what I understand, I need to interface the control card with CCS using the onboard JTAG found on the DRV8312.  That is as far as I have come.  Can you please provide some information on how to do this ? What other component would I need?  I also have this kit:  C2000 Piccolo MCU F280049C LaunchPad™ development kit.  

 


Thanks so much! 

AR