I would like to detect an rising comparator output and execute an interrupt routine for that rising comparator output.
I found that I can do this by connecting the compout pin to another gpio and configuring that gpio as an xint source..
However if I wanna save some pins. can I just configure the compout pin as an xint input and do two things on the same pin ( i.e. use the same pin for both compout and xint input)
Thanks in advance.