This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
GPIO63 goes to J6 pin 55. It also goes to U2 pin6. When I grounded OE on U2 pin8. the glitch went away.
Bob,
Can you elaborate a bit more here? I am not sure what the problem is other than you saying that there is a glitch that goes away when you ground U2.
- What are you trying to accomplish?
- Is there application code running during a glitch?
- What affect does this glitch have on your system?
If you can share a bit more information, we might be able to assist better.
Thanks,
Mark
Bob,
I am not sure if you resolved this issue, but someone else posted the exact same question a few days ago. I was able to get my hands on a board and debug myself. I confirmed that there is something funky going on with the level shifter. I modified a board to tie OE to gnd and disable the levelshifter. It resolves the problem as you say. I will be filing a bug to get this looked and and find the root cause. In the meantime, if you do not plan on using the levelshifter, you may either want to remove it completely or just tie OE to GND.
Here is the link to the second post:
e2e.ti.com/.../556520
If you have any more questions don't hesitate to create a new post.
Regards,
Mark