Our project needs to allow the upgrade of the application code via a serial port.
In the past we have written a custom boot loader and installed it in flash and it will down load application serially and program into flash and jump to the application.
Is there a way to use the built in boot loader serial interface to perform this operation on a F28377S Delfino?
If so is there an example application and or documentation that explains how to send a hex or out file to the boot loader?
Thanks
Maury