This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
for reference code
#include "DSP28x_Project.h" // Device Headerfile
// Prototype statements for functions found within this file.
void InitEPwm4n5(void);
void InitEPwm2(void);
void InitEPwm3(void);
__interrupt void epwm2_isr(void);
__interrupt void epwm3_isr(void);
__interrupt void adc_isr(void);
void Adc_Config(void);
typedef struct
{
volatile struct EPWM_REGS *EPwmRegHandle4;
volatile struct EPWM_REGS *EPwmRegHandle5;
volatile struct EPWM_REGS *EPwmRegHandle2;
volatile struct EPWM_REGS *EPwmRegHandle3;
Uint16 TBPRD;
Uint16 Duty_Set;
Uint16 MAX_CMP;
Uint16 MIN_CMP;
Uint16 DB_Set;
Uint16 Delay_Set;
Uint16 EPwmTimerIntCountP;
Uint16 EPwmTimerIntCountC;
}EPWM_INFO;
void add_Miss_Pulse_P(EPWM_INFO*);
void add_Miss_Pulse_C(EPWM_INFO*);
//
#define TBCLK 60000 // Don't change
#define STEP_UP_DOWN 0 // if 0, delay in PWM2 and PWM3 else delay in PWM1
#define FREQ 100 // KHZ
#define DB 200 // ns (better in multiples of 50ns)
#define DELAY 200 // ns (better in multiples of 50ns)
#define PULSE_MISS_FREQ 100 // Miss PULSE_MISS no. per PULSE_MISS_FREQ
#define PULSE_MISS 1 // No. of pulses to remove
EPWM_INFO epwm_info;
Uint16 LoopCount;
Uint16 ConversionCount;
Uint16 VoltageADC;
double actualVoltage=0;
void main(void)
{
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
InitSysCtrl();
// Step 2. Initialize GPIO:
// This example function is found in the DSP2803x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
// InitGpio(); // Skipped for this example
// For this case just init GPIO pins for ePWM1, ePWM2, ePWM3
// These functions are in the DSP2803x_EPwm.c file
InitEPwm2Gpio();
InitEPwm3Gpio();
InitEPwm4Gpio();
InitEPwm5Gpio();
InitAdc();
AdcOffsetSelfCal();
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
DINT;
// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the DSP2803x_PieCtrl.c file.
InitPieCtrl();
// Disable CPU interrupts and clear all CPU interrupt flags:
IER = 0x0000;
IFR = 0x0000;
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in DSP2803x_DefaultIsr.c.
// This function is found in DSP2803x_PieVect.c.
InitPieVectTable();
EALLOW; // This is needed to write to EALLOW protected registers
PieVectTable.EPWM2_INT = &epwm2_isr;
PieVectTable.EPWM3_INT = &epwm3_isr;
PieVectTable.ADCINT1 = &adc_isr;
EDIS; // This is needed to disable write to EALLOW protected registers
// Initialize all the Device Peripherals:
// Not required for this example
EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0;
EDIS;
epwm_info.TBPRD = TBCLK/(FREQ*2);
epwm_info.DB_Set = DB*3/50;
epwm_info.Delay_Set = DELAY*3/50;
epwm_info.Duty_Set = epwm_info.TBPRD/2;
epwm_info.MAX_CMP = epwm_info.TBPRD;
epwm_info.MIN_CMP = 0;
InitEPwm4n5();
InitEPwm2();
InitEPwm3();
InitAdc();
AdcOffsetSelfCal();
EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1;
EDIS;
// Enable CPU INT3 which is connected to EPWM1-3 INT:
IER |= M_INT3;
// Enable ADCINT1 in PIE
PieCtrlRegs.PIEIER1.bit.INTx1 = 1; // Enable INT 1.1 in the PIE
IER |= M_INT1; // Enable CPU Interrupt 1
// Enable EPWM INTn in the PIE: Group 3 interrupt 1-3
PieCtrlRegs.PIEIER3.bit.INTx2 = 1;
PieCtrlRegs.PIEIER3.bit.INTx3 = 1;
// Enable global Interrupts and higher priority real-time debug events:
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
// Configure ADC
// Note: Channel ADCINA1 will be double sampled to workaround the ADC 1st sample issue for rev0 silicon errata
EALLOW;
AdcRegs.ADCCTL1.bit.INTPULSEPOS = 1; //ADCINT1 trips after AdcResults latch
AdcRegs.INTSEL1N2.bit.INT1E = 1; //Enabled ADCINT1
AdcRegs.INTSEL1N2.bit.INT1CONT = 0; //Disable ADCINT1 Continuous mode
AdcRegs.INTSEL1N2.bit.INT1SEL = 2; //setup EOC2 to trigger ADCINT1 to fire
AdcRegs.ADCSOC0CTL.bit.CHSEL = 1; //set SOC0 channel select to ADCINA1(dummy sample for rev0 errata workaround)
AdcRegs.ADCSOC1CTL.bit.CHSEL = 1; //set SOC1 channel select to ADCINA1
AdcRegs.ADCSOC2CTL.bit.CHSEL = 2; //set SOC2 channel select to ADCINA2
AdcRegs.ADCSOC0CTL.bit.TRIGSEL = 5; //set SOC0 start trigger on EPWM1A, due to round-robin SOC0 converts first then SOC1, then SOC2
AdcRegs.ADCSOC1CTL.bit.TRIGSEL = 5; //set SOC1 start trigger on EPWM1A, due to round-robin SOC0 converts first then SOC1, then SOC2
AdcRegs.ADCSOC2CTL.bit.TRIGSEL = 5; //set SOC2 start trigger on EPWM1A, due to round-robin SOC0 converts first then SOC1, then SOC2
AdcRegs.ADCSOC0CTL.bit.ACQPS = 6; //set SOC0 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
AdcRegs.ADCSOC1CTL.bit.ACQPS = 6; //set SOC1 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
AdcRegs.ADCSOC2CTL.bit.ACQPS = 6; //set SOC2 S/H Window to 7 ADC Clock Cycles, (6 ACQPS plus 1)
EDIS;
// Assumes ePWM1 clock is already enabled in InitSysCtrl();
EPwm1Regs.ETSEL.bit.SOCAEN = 1; // Enable SOC on A group
EPwm1Regs.ETSEL.bit.SOCASEL = 4; // Select SOC from from CPMA on upcount
EPwm1Regs.ETPS.bit.SOCAPRD = 1; // Generate pulse on 1st event
EPwm1Regs.CMPA.half.CMPA = 0x0080; // Set compare A value
EPwm1Regs.TBPRD = 0xFFFF; // Set period for ePWM1
EPwm1Regs.TBCTL.bit.CTRMODE = 0; // count up and start
// Step 6. IDLE loop. Just sit and loop forever (optional):
for(;;)
{
LoopCount++;
__asm(" NOP");
}
}
void InitEPwm4n5()
{
EPwm4Regs.TBPRD = epwm_info.TBPRD; // Set timer period
EPwm4Regs.TBPHS.half.TBPHS = 0x0000; // Phase is 0
EPwm4Regs.TBCTR = 0x0000; // Clear counter
EPwm5Regs.TBPRD = epwm_info.TBPRD; // Set timer period
EPwm5Regs.TBPHS.half.TBPHS = 0x0000; // Phase is 0
EPwm5Regs.TBCTR = 0x0000; // Clear counter
// Setup TBCLK pwm4
EPwm4Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up
EPwm4Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Disable phase loading
//EPwm4Regs.TBCTL.bit.SYNCOSEL = TB_CTR_ZERO; // Sync down-stream module
EPwm4Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // Clock ratio to SYSCLKOUT
EPwm4Regs.TBCTL.bit.CLKDIV = TB_DIV1;
EPwm4Regs.CMPCTL.bit.SHDWAMODE = CC_IMMEDIATE; // Load registers ZERO
EPwm4Regs.CMPCTL.bit.SHDWBMODE = CC_IMMEDIATE;
// Setup TBCLK pwm5
EPwm5Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up
EPwm5Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Disable phase loading
//EPwm5Regs.TBCTL.bit.PHSDIR = TB_UP; // Count DOWN on sync
//EPwm5Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN; // sync flow-through
EPwm5Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // Clock ratio to SYSCLKOUT
EPwm5Regs.TBCTL.bit.CLKDIV = TB_DIV1;
EPwm5Regs.CMPCTL.bit.SHDWAMODE = CC_IMMEDIATE; // Load registers imm
EPwm5Regs.CMPCTL.bit.SHDWBMODE = CC_IMMEDIATE;
// Setup compare PWM4
if(!STEP_UP_DOWN)
{
EPwm4Regs.CMPA.half.CMPA = epwm_info.Duty_Set;//150
}
else
{
EPwm4Regs.CMPA.half.CMPA = epwm_info.Duty_Set - epwm_info.Delay_Set; //138
}
// Setup compare pwm5
if(!STEP_UP_DOWN)
{
EPwm5Regs.CMPA.half.CMPA = epwm_info.Duty_Set;//150
}
else
{
EPwm5Regs.CMPA.half.CMPA = epwm_info.Duty_Set + epwm_info.Delay_Set; //162
}
// Set actions
EPwm5Regs.AQCTLA.bit.CAU = AQ_SET; //
EPwm5Regs.AQCTLA.bit.CAD = AQ_CLEAR; //
EPwm4Regs.AQCTLA.bit.CAU = AQ_CLEAR; //
EPwm4Regs.AQCTLA.bit.CAD = AQ_SET; //
// Active High COMP PWMs - Setup Deadband
EPwm5Regs.DBCTL.bit.OUT_MODE = DBA_ENABLE;
EPwm5Regs.DBCTL.bit.POLSEL = DB_ACTV_HI;
EPwm5Regs.DBCTL.bit.IN_MODE = DBA_RED_DBB_FED;
EPwm5Regs.DBRED = epwm_info.DB_Set;
EPwm5Regs.DBFED = epwm_info.DB_Set;
EPwm4Regs.DBCTL.bit.OUT_MODE = DBA_ENABLE;
EPwm4Regs.DBCTL.bit.POLSEL = DB_ACTV_HI;
EPwm4Regs.DBCTL.bit.IN_MODE = DBA_RED_DBB_FED;
EPwm4Regs.DBRED = epwm_info.DB_Set;
EPwm4Regs.DBFED = epwm_info.DB_Set;
epwm_info.EPwmTimerIntCountP = 0;
epwm_info.EPwmTimerIntCountC = 0;
epwm_info.EPwmRegHandle4 = &EPwm4Regs; // Set the pointer to the ePWM module
epwm_info.EPwmRegHandle5 = &EPwm5Regs; // Set the pointer to the ePWM module
}
void InitEPwm2()
{
EPwm2Regs.TBPRD = epwm_info.TBPRD; // Set timer period
EPwm2Regs.TBPHS.half.TBPHS = 0x0000; // Phase is 0
EPwm2Regs.TBCTR = 0x0000; // Clear counter
// Setup TBCLK
EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up
EPwm2Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Disable phase loading
//EPwm2Regs.TBCTL.bit.PHSDIR = TB_UP; // Count DOWN on sync
//EPwm2Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN; // sync flow-through
EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // Clock ratio to SYSCLKOUT
EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV1; // Slow just to observe on the scope
EPwm2Regs.CMPCTL.bit.SHDWAMODE = CC_IMMEDIATE;
EPwm2Regs.CMPCTL.bit.SHDWBMODE = CC_IMMEDIATE;
// Setup compare
if(!STEP_UP_DOWN)
{
EPwm2Regs.CMPA.half.CMPA = epwm_info.Duty_Set-epwm_info.Delay_Set; //138
EPwm2Regs.CMPB = epwm_info.Duty_Set+epwm_info.Delay_Set; //162
}
else
{
EPwm2Regs.CMPA.half.CMPA = epwm_info.Duty_Set;//150
EPwm2Regs.CMPB = epwm_info.Duty_Set;//150
}
// Set actions
EPwm2Regs.AQCTLA.bit.CAU = AQ_CLEAR; // Set PWM2A on CAU
EPwm2Regs.AQCTLA.bit.CAD = AQ_SET; // Clear PWM2A on CAD
EPwm2Regs.AQCTLB.bit.CBU = AQ_CLEAR; // Clear PWM2B on CAU
EPwm2Regs.AQCTLB.bit.CBD = AQ_SET; // Set PWM2B on CAD
EPwm2Regs.ETSEL.bit.INTSEL = ET_CTR_ZERO; // Select INT on Zero event
EPwm2Regs.ETSEL.bit.INTEN = 1; // Enable INT
EPwm2Regs.ETPS.bit.INTPRD = ET_1ST; // Generate INT on 1st event
// Active Low complementary PWMs - setup the deadband
EPwm2Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;
EPwm2Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC;
EPwm2Regs.DBCTL.bit.IN_MODE = DBA_RED_DBB_FED;
EPwm2Regs.DBRED = epwm_info.DB_Set;
EPwm2Regs.DBFED = epwm_info.DB_Set;
epwm_info.EPwmRegHandle2 = &EPwm2Regs; // Set the pointer to the ePWM module
}
void InitEPwm3()
{
EPwm3Regs.TBPRD = epwm_info.TBPRD; // Set timer period
EPwm3Regs.TBPHS.half.TBPHS = 0x0000; // Phase is 0
EPwm3Regs.TBCTR = 0x0000; // Clear counter
// Setup TBCLK
EPwm3Regs.TBCTL.bit.CTRMODE = TB_COUNT_UPDOWN; // Count up
EPwm3Regs.TBCTL.bit.PHSEN = TB_DISABLE; // Disable phase loading
//EPwm3Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN; // sync flow-through
//EPwm3Regs.TBCTL.bit.PHSDIR = TB_UP; // Count DOWN on sync
EPwm3Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1; // Clock ratio to SYSCLKOUT
EPwm3Regs.TBCTL.bit.CLKDIV = TB_DIV1; // Slow just to observe on the scope
EPwm3Regs.CMPCTL.bit.SHDWAMODE = CC_IMMEDIATE;
EPwm3Regs.CMPCTL.bit.SHDWBMODE = CC_IMMEDIATE;
// Setup compare
if(!STEP_UP_DOWN)
{
EPwm3Regs.CMPA.half.CMPA = epwm_info.Duty_Set+epwm_info.Delay_Set; //162
EPwm3Regs.CMPB = epwm_info.Duty_Set-epwm_info.Delay_Set; //138
}
else
{
EPwm3Regs.CMPA.half.CMPA = epwm_info.Duty_Set;//150
EPwm3Regs.CMPB = epwm_info.Duty_Set;//150
}
// Set actions
EPwm3Regs.AQCTLA.bit.CAU = AQ_SET; // Set PWM2A on CAU
EPwm3Regs.AQCTLA.bit.CAD = AQ_CLEAR; // Clear PWM2A on CAD
EPwm3Regs.AQCTLB.bit.CBU = AQ_SET; // Clear PWM2B on CAU
EPwm3Regs.AQCTLB.bit.CBD = AQ_CLEAR; // Set PWM2B on CAD
EPwm3Regs.ETSEL.bit.INTSEL = ET_CTR_PRD; // Select INT on Period event
EPwm3Regs.ETSEL.bit.INTEN = 1; // Enable INT
EPwm3Regs.ETPS.bit.INTPRD = ET_1ST; // Generate INT on 1st event
// Active Low complementary PWMs - setup the deadband
EPwm3Regs.DBCTL.bit.OUT_MODE = DB_FULL_ENABLE;
EPwm3Regs.DBCTL.bit.POLSEL = DB_ACTV_HIC;
EPwm3Regs.DBCTL.bit.IN_MODE = DBA_RED_DBB_FED;
EPwm3Regs.DBRED = epwm_info.DB_Set;
EPwm3Regs.DBFED = epwm_info.DB_Set;
epwm_info.EPwmRegHandle3 = &EPwm3Regs; // Set the pointer to the ePWM module
}
__interrupt void epwm2_isr(void)
{
// Update the CMP values
add_Miss_Pulse_P(&epwm_info);
// Clear INT flag for this timer
EPwm2Regs.ETCLR.bit.INT = 1;
// Acknowledge this interrupt to receive more interrupts from group 3
PieCtrlRegs.PIEACK.all = PIEACK_GROUP3;
}
__interrupt void epwm3_isr(void)
{
// Update the CMP values
add_Miss_Pulse_C(&epwm_info);
// Clear INT flag for this timer
EPwm3Regs.ETCLR.bit.INT = 1;
// Acknowledge this interrupt to receive more interrupts from group 3
PieCtrlRegs.PIEACK.all = PIEACK_GROUP3;
}
__interrupt void adc_isr(void)
{
VoltageADC = AdcResult.ADCRESULT1; //discard ADCRESULT0 as part of the workaround to the 1st sample errata for rev0
/*int i = 0;
while (i < 32 && Voltage1 <= temp_table[i])
{
i++;
}
double m = 1.0/(temp_table[i]-temp_table[i-1]);
double c = i - m*temp_table[i];
temperature = 4*(m*Voltage1 + c);*/
AdcRegs.ADCINTFLGCLR.bit.ADCINT1 = 1; //Clear ADCINT1 flag reinitialize for next SOC
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1; // Acknowledge interrupt to PIE
return;
}
int mp = 0;
int mc = 0;
int enablep = 0;
int enablec = 0;
void add_Miss_Pulse_P(EPWM_INFO *epwm_infoF)
{
if(epwm_infoF->EPwmTimerIntCountP == PULSE_MISS_FREQ - PULSE_MISS-1)
{
epwm_infoF->EPwmTimerIntCountP = 0;
mp=0;
enablep = 1;
//epwm_infoF->EPwmRegHandle2->CMPA.half.CMPA = epwm_info.MIN_CMP;
epwm_infoF->EPwmRegHandle2->CMPB = epwm_info.MAX_CMP;
epwm_infoF->EPwmRegHandle3->CMPA.half.CMPA = epwm_info.MAX_CMP;
//epwm_infoF->EPwmRegHandle3->CMPB = epwm_info.MIN_CMP;
//epwm_infoF->EPwmRegHandle4->CMPA.half.CMPA = epwm_info.MIN_CMP;
epwm_infoF->EPwmRegHandle5->CMPA.half.CMPA = epwm_info.MAX_CMP;
}
else if(enablep)
{
mp++;
if(mp == PULSE_MISS)
{
enablep=0;
//epwm_infoF->EPwmRegHandle2->CMPA.half.CMPA = (!STEP_UP_DOWN)? epwm_info.Duty_Set - epwm_info.Delay_Set : epwm_info.Duty_Set;
epwm_infoF->EPwmRegHandle2->CMPB = (!STEP_UP_DOWN)?epwm_info.Duty_Set + epwm_info.Delay_Set : epwm_info.Duty_Set;
epwm_infoF->EPwmRegHandle3->CMPA.half.CMPA = (!STEP_UP_DOWN)? epwm_info.Duty_Set + epwm_info.Delay_Set : epwm_info.Duty_Set;
//epwm_infoF->EPwmRegHandle3->CMPB = (!STEP_UP_DOWN)?epwm_info.Duty_Set - epwm_info.Delay_Set : epwm_info.Duty_Set;
//epwm_infoF->EPwmRegHandle4->CMPA.half.CMPA = (!STEP_UP_DOWN)? epwm_info.Duty_Set : epwm_info.Duty_Set - epwm_info.Delay_Set;
epwm_infoF->EPwmRegHandle5->CMPA.half.CMPA = (!STEP_UP_DOWN)? epwm_info.Duty_Set : epwm_info.Duty_Set + epwm_info.Delay_Set;
}
}
else
++epwm_infoF->EPwmTimerIntCountP;
return;
}
void add_Miss_Pulse_C(EPWM_INFO *epwm_infoF)
{
if(epwm_infoF->EPwmTimerIntCountC == PULSE_MISS_FREQ -PULSE_MISS - 1)
{
epwm_infoF->EPwmTimerIntCountC = 0;
mc=0;
enablec = 1;
epwm_infoF->EPwmRegHandle2->CMPA.half.CMPA = epwm_info.MIN_CMP;
//epwm_infoF->EPwmRegHandle2->CMPB = epwm_info.MAX_CMP;
//epwm_infoF->EPwmRegHandle3->CMPA.half.CMPA = epwm_info.MAX_CMP;
epwm_infoF->EPwmRegHandle3->CMPB = epwm_info.MIN_CMP;
epwm_infoF->EPwmRegHandle4->CMPA.half.CMPA = epwm_info.MIN_CMP;
//epwm_infoF->EPwmRegHandle5->CMPA.half.CMPA = epwm_info.MAX_CMP;
}
else if(enablec)
{
mc++;
if(mc == PULSE_MISS)
{
enablec=0;
//++epwm_infoF->EPwmTimerIntCountC;
epwm_infoF->EPwmRegHandle2->CMPA.half.CMPA = (!STEP_UP_DOWN)? epwm_info.Duty_Set - epwm_info.Delay_Set : epwm_info.Duty_Set;
//epwm_infoF->EPwmRegHandle2->CMPB = (!STEP_UP_DOWN)?epwm_info.Duty_Set + epwm_info.Delay_Set : epwm_info.Duty_Set;
//epwm_infoF->EPwmRegHandle3->CMPA.half.CMPA = (!STEP_UP_DOWN)? epwm_info.Duty_Set + epwm_info.Delay_Set : epwm_info.Duty_Set;
epwm_infoF->EPwmRegHandle3->CMPB = (!STEP_UP_DOWN)?epwm_info.Duty_Set - epwm_info.Delay_Set : epwm_info.Duty_Set;
epwm_infoF->EPwmRegHandle4->CMPA.half.CMPA = (!STEP_UP_DOWN)? epwm_info.Duty_Set : epwm_info.Duty_Set - epwm_info.Delay_Set;
//epwm_infoF->EPwmRegHandle5->CMPA.half.CMPA = (!STEP_UP_DOWN)? epwm_info.Duty_Set : epwm_info.Duty_Set + epwm_info.Delay_Set;
}
}
else
++epwm_infoF->EPwmTimerIntCountC;
return;
}
Laskshmi,
after syncing ePWM 2a or 2b where do you see this extra delay? For example: Has the signals period increased? A longer or shorter ontime/offtime? Or is it a delta between two ePWMs that should be synced, and if so and what is your expected value and what value are you seeing?
Regards,
Cody
Hey
there 6 signals
5a and 4a are comlepentry with dead band 200ns and 50% duty
2b and 2a are complementry with deadband 200ns and duty is such that 2b rising edge(RE) is after 200ns of 5a RE and falling edge(FE) is 200ns before FE of 5a. but i am getting 200ns +16.66ns and 200ns- 16.66ns respectively on 2b. similarly 2a and 4a but 200ns is correct. but pulse width remains same in both cases.
3a and 3b are complementry. have similar issue here too.
Lakshmi,
since you used ControlSuite header files I was able to build your code, note any changes you made to the header files I will cause differences between the code I tested and what you are using. I do NOT see the delay you are talking about.
I verified the following:
2b -> 5a is 200ns for both falling and rising edges
2a-> 5a is 400ns on between both transitions
2b-> 2a is 600ns for both transitions
3a=2b
3b=2a
All numbers I measured were very close to even values of 100. Of course if you measure the 0% transition level of one signal and the 100% transition level of the next signal your measurement will be longer than expected. Can you verify your measurements always measuring the delay between transitions at 1.65V(50% through the transition)?
Regards,
Cody
LT,
i am still not seeing this issue, this could be a small code difference or even compiler settings. Can you send me what compiler version you are using and the optimization settings? Secondly, if possible please send me your .out file, I can then check if I observe the same discrepancy as you on my hardware setup.
Note: You can directly attach the .out file to your post.
Regards,
Cody
Cody,
I uploaded the screen shots of compiler version using and the optimization settings. Also the out file too in the same folder.
drive.google.com/open
Regards,
LT
LT,
I currently don’t know what is causing the difference, you will need to debug that in your code. However, The differences between your desired code, and the .out file you compiled and sent to me are as follows:
Parameter : Good setting --Bad setting
ePWM2 CMPA : 0x8A0000 --0x870000
ePWM2 CMPB :0xA2 --0xA5
ePWM2 DBRED :0x0C --0x18
ePWM2 DBFED :0x0C --0x18
ePWM5 DBRED :0x0C --0x18
ePWM5 DBFED :0x0C --0x18
NOTE: the good settings are from my working code, and the “bad settings” are what are found in the registers when I run your .out file.
NOTE: I did not list all discrepancies just the relevant ones for ePWM 2 and ePWM5.
When I forced the working code to the “bad settings” above I see the same behavior when using the .out you sent me. This should at least tell you what to look at in your code.
Hope it helps,
Cody
LT,
have you found out what was causing these small differences? If so, please post so other can avoid your issue in the future!
Regards,
Cody