This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am using TI InstaSpin FOC software on a TMS320F28069M, integrated in a high voltage board with PMSM motor.
In our application, the motor is coupled with a high speed fan.
The fan could be driven by the medium, also if the motor is unpowered.
I am looking for a hint, how to start the instaspin FOC routines, if there is already a certain speed on the motor.
It is clear, that it does not make sense, to use recalibration routines (e.g. for motorresistance or offset-values),
because of the routines would apply measure-currents to the spinning motor.
Is it only an issue to provide the detected motorspeed as target speed to the rpm-controller?
Regards
Martin Bayer
Hi Yanming,
For flying start, when the motor is spin in the same rotation direction with our driver, it's good.
BUT, when the motor is initially spin in the opposite direction, the main voltage would increase from 320 to 380 in short time.
Could you help advise? Thanks!