This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
I am facing this problem when using TMS320F28027. I have tried to replace the MCU but still the same problem. My PCB follows the reference design from TI. I pull the XRS pin to VDD 3.3V via 2K2 resistor but when i measure it, the voltage keep at zero.
Plz help!
C28xx: Failed CPU Reset: (Error -1137 @ 0x6) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 6.0.576.0)
C28xx: Trouble Reading Register PC: (Error -1137 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 6.0.576.0)
C28xx: Trouble Reading Register ST1: (Error -1137 @ 0x6) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 6.0.576.0)
C28xx: GEL: Error while executing OnReset(1): Target failed to read register ST1
at (ST1&~(0x0100)) [f28027.gel:283]
at C28x_Mode() [f28027.gel:33]
at OnReset(1)
C28xx: Flash Programmer: Warning: The configured device (TMS320F28027), does not match the detected device (). Flash Programming operations could be affected. Please consider modifying your target configuration file.
C28xx: Failed CPU Reset: (Error -1137 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 6.0.576.0)
C28xx: Trouble Reading Register PC: (Error -1137 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 6.0.576.0)
C28xx: Trouble Reading Register ST1: (Error -1137 @ 0x6) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 6.0.576.0)
C28xx: GEL: Error while executing OnReset(1): Target failed to read register ST1
at (ST1&~(0x0100)) [f28027.gel:283]
at C28x_Mode() [f28027.gel:33]
at OnReset(1)
C28xx: Trouble Writing Memory Block at 0x0 on Page 0 of Length 0x2: (Error -1137 @ 0x6) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 6.0.576.0)
C28xx: File Loader: Verification failed: Target failed to write 0x00000@Program
C28xx: GEL: File: C:\Users\bebo_\workspace\Example_F2802xEPwmDCEventTripComp\RAM\Example_F2802xEPwmDCEventTripComp.out: Load failed.
Hi,
Quynh Chi88 said:I pull the XRS pin to VDD 3.3V via 2K2 resistor but when i measure it, the voltage keep at zero.
That's the matter of concern! Can you check your design for any short? Any test points for 3.3V? Check the voltages.
Regards,
Gautam