Part Number: TMDSSOLARPEXPKIT
Hi, there!
I have found several lab-environment test bed with TMDSSOLARCEXPKIT --- Concerto-based Solar Explorer Development Kit, but this set can only handle a 50W solar input.
While I was trying to find similar board that could handle larger power ratings, I found TMDSHVMPPTKIT --- High Voltage Isolated Solar MPPT Developers Kit, which provides 400 DC output. It says that working with TMSHV1PHINVKIT, it could provide AC output. However the latter, TMSHV1PHINVKIT, seems to be not available any more.
Basically I was trying to build a microgrid power system prototype, it has pv input, battery storage, DC-DC converter with MPPT, DC-AC inverter, and connect to grid. The system will be a scaled down version, but I am not sure if a 50W PV system, if I use TMDSSOLARCEXPKIT --- Concerto-based Solar Explorer Development Kit, was scaled too much. Will that be the case?
Thanks!