I work with a TI piccolo TMS320F28027. I have a problem that I can’t explain yet without your help. I think it is the duty cycle range limitation who cause my problem:
My scheme is a buck converter control by the MCU. I try to put duty cycle to 0 to ensure inhibition of buck. I am in standby Mode. In all the product we made (more than 30000), I don’t see my problem except on one product. I see a duty cycle of 50ns every 0,5ms (2KHz). My switch frequency is at 100KHz. I don’t understand this little pulse at 2KHz. Perhaps it come from the duty cycle range limitation where the first three cycle are undefined behavior on the ePWMxA output.
So is this duty cycle range limitation could create a repetitive duty cycle when I want 0%? Is it repeatable or random?