This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello there,
i have created a project for the TMS320F23879D on the LaunchXL board from scratch using
CCS Version 6.2.0.00050
by
FILE > NEW > CCS Project > Empty Project
and the application dosen´t start after flashing.
Earlier it did, and i never changed the positions of the boot select pins of the LaunchPad.
By earlier i mean that after a vacation i had to set up CCS freshly, since to some automatic network maintance it didn´t work anymore.
It runs when i use debugging and i see CCS writes the code to flash, but when i exit the debug modus and reset the device power on-off or the
reset button, ths application doesn´t start.
I read in the manual about the Z1 and Z2 zones in the DCSM area. I "screenshoted" the content, see below.
Does someone have hint, why the application doesn´t start?
PS.: i had an earlier thread, and i was told to shift this topic to this forum
e2e.ti.com/.../636742
Best regards!!