This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28379D: Detailed dimensions of the LaunchPad

Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: C2000WARE

Dear friends,

I searched, but I couldn't find the detailed dimensions of the F28379D LaunchPad. In another thread, there is the dimensions only of the PCB itself, not the pin headers. The Tiva C Series TM4C123G LaunchPad have the following picture in its user's guide:

There is something like this for the LAUNCHXL-F28379D? If not, what are the distances between the pin headers, horizontally (in the case above, 1600 mil) and vertically? 

Thank you in advance,

Gabriel Pauka

  • Gabriel,
    At the moment we don't have the mechanical drawings for all of those dimensions. I will see if this is something we can add in the future.

    The LaunchPad standard defines the BoosterPack headers to be 1800mil and 1600mil spacing between outer and inner connection connectors. This is true for All LaunchPads for sale by TI. Please let me know if there are any additional measurements that you are specifically looking for.

    Thanks,
    Mark
  • Thank you, Mark.

    For now, I just need the "vertical distance" between the headers, the "A" and "B" in the picture below. Can you provide me these values? I am designing a PCB that will have the LAUNCHXL-F28379D on it, so I really need to place all the four headers precisely.

  • Gabriel,

    The design files are available in C2000Ware. This board was created with Altium Designer. Feel free to open the files up yourself and make any measurement you need.

    The dimensions you are looking for are measured from the center of the pins.
    A: 1600 mil
    B: 3400 mil


    Thanks,
    Mark
  • Thank you Mark!

    That is exactly what I was looking for.