This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hello,
I am using 28035 Piccolo on a custom board. I am trying to flash my code to 28035 using JTAG connection. I was able to flash the code and suddenly it shows error : Failed CPU Reset: (Error -1137 @ 0x6).
Can someone explain what is the problem and what could be a possible solution to fix it?
What is the procedure for putting device in wait boot mode! And how to check if device is locked?
Thanks
Sagar
Sagar,
Wait boot mode:Pg 16, Table 4
GPIO37 should be pulled high & GPIO34 should be pulled low to get into wait boot mode.
How to check whether device is locked?
Check bit 0 of CSMSCR. If this bit is 1, then device is locked.
Regards,
Manoj