Part Number: INSTASPINUNIVERSALGUI
Other Parts Discussed in Thread: MOTORWARE
For INSTASPINUNIVERSALGUI the documentation talks about running the GUI in standalone mode or inside of CCS.
I typically use the GUI inside of CCS as it is simpler than using the Expressions View and quickly gives me more visibility of the project.
With CCSv7 - due to a change in the GUI Composer component - if trying to use inside of CCS the existing documentation is no longer accurate.
Here is what you will need to do to get this to work for CCSv7 (and in the future I would assume with CCSv8 etc.)
View --> CCS App Center
search for: GUI
Select: GUI Composer Runtime
Install Software
Restart CCS
Copy your INSTASPINUNIVERSAL 'webapps' folder from
C:\ti\guicomposer
to the CCSv7 installation folder
C:\ti\ccsv7
Restart CCS
Now you should see
View --> GUI Composer --> Applications v1 --> InstaSPIN_F2806xM_UNIVERSAL (and the F2802x and F2805x)
Select any of these (it does not matter if it matches the F280x device you are using)
And you can follow the standard user guide @
C:\ti\motorware\motorware_1_01_00_18\docs\guis\universal
-Chris