Part Number: TMS320F28027
Other Parts Discussed in Thread: C2000WARE
Hello,
With conventional PWM operation at 500 kHz, the best phase shift granularity I can achieve between two PWM signals in the sync chain is 3° (with SYSCLKOUT = 60 MHz). For my application I need better phase shift granularity, but am having trouble getting phase shift operation to work with the High Resolution PWM.
The relevant code I have is shown below. Can someone help me achieve HRPWM phase shift and/or explain to me why this code does not work?
EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 0;
EDIS;
//configure ePWM1
Uint16 period = 120; // 60MHz/120 = 500 kHz
EPwm1Regs.TBPRD = period-1; // PWM frequency = 1 / period
EPwm1Regs.CMPA.half.CMPA = period/2; // set duty 50% initially
EPwm1Regs.CMPA.half.CMPAHR = (0 << 8); // initialize HRPWM extension
EPwm1Regs.TBPHS.half.TBPHS = 0; // initialize coarse phase to 0
EPwm1Regs.TBCTR = 0;
EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP; // count up mode
EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE; // EPwm1 is the Master
EPwm1Regs.TBCTL.bit.PRDLD = TB_SHADOW; // set Immediate load
EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_CTR_ZERO;
EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;
EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV1;
EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
EPwm1Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
EPwm1Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm1Regs.AQCTLA.bit.ZRO = AQ_SET; // High/low behavior on ePWM1
EPwm1Regs.AQCTLA.bit.CAU = AQ_CLEAR;
EALLOW;
EPwm1Regs.HRCNFG.all = 0x0;
EPwm1Regs.HRCNFG.bit.HRLOAD = HR_CTR_ZERO; // HR_CTR_ZERO_PRD; // Load on CTR = 0 and CTR = TBPRD
EPwm1Regs.HRCNFG.bit.AUTOCONV = 1; // Enable autoconversion for HR period
EPwm1Regs.HRCNFG.bit.EDGMODE = HR_BEP; // MEP control on both edges
EPwm1Regs.HRCNFG.bit.CTLMODE = HR_PHS; // Selects the register (CMP/TBPRD or TBPHS) that controls the MEP:
EPwm1Regs.HRPCTL.bit.TBPHSHRLOADE = 1; // This bit allows you to synchronize ePWM modules with a high-resolution phase on a SYNCIN event
EPwm1Regs.TBCTL.bit.PHSDIR = 1; // count up after SYNC event and the new value of the phase (TBPHS) is loaded.
EPwm1Regs.HRPCTL.bit.HRPE = 1; // Enable high-resolution period control.
EDIS;
//configure ePWM2
EPwm2Regs.TBPRD = period-1; // PWM frequency = 1 / period
EPwm2Regs.CMPA.half.CMPA = period/2; // set duty 50% initially
EPwm2Regs.CMPA.half.CMPAHR = (0 << 8); // initialize HRPWM extension
EPwm2Regs.TBPHS.half.TBPHS = 0;
EPwm2Regs.TBCTR = 0;
EPwm2Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP;
EPwm2Regs.TBCTL.bit.PHSEN = TB_ENABLE;
EPwm2Regs.TBCTL.bit.PRDLD = TB_SHADOW; // set Immediate load
EPwm2Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_IN; // EPwm2 is the slave
EPwm2Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;
EPwm2Regs.TBCTL.bit.CLKDIV = TB_DIV1;
EPwm2Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;
EPwm2Regs.CMPCTL.bit.LOADBMODE = CC_CTR_ZERO;
EPwm2Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
EPwm2Regs.CMPCTL.bit.SHDWBMODE = CC_SHADOW;
EPwm2Regs.AQCTLA.bit.ZRO = AQ_SET;
EPwm2Regs.AQCTLA.bit.CAU = AQ_CLEAR;
EALLOW;
EPwm2Regs.HRCNFG.all = 0x0;
EPwm2Regs.HRCNFG.bit.HRLOAD = HR_CTR_ZERO; //HR_CTR_ZERO_PRD; // Load on CTR = 0 and CTR = TBPRD
EPwm2Regs.HRCNFG.bit.AUTOCONV = 1; // Enable autoconversion for HR period
EPwm2Regs.HRCNFG.bit.EDGMODE = HR_BEP; // MEP control on both edges
EPwm2Regs.HRCNFG.bit.CTLMODE = HR_PHS; // Selects the register (CMP/TBPRD or TBPHS) that controls the MEP:
EPwm2Regs.HRPCTL.bit.TBPHSHRLOADE = 1; // This bit allows you to synchronize ePWM modules with a high-resolution phase on a SYNCIN event
EPwm2Regs.TBCTL.bit.PHSDIR = 1; // count up after SYNC event and the new value of the phase (TBPHS) is loaded.
EPwm2Regs.HRPCTL.bit.HRPE = 1; // Enable high-resolution period control.
EDIS;
//set the phase registers of ePWM2
EPwm2Regs.TBPHS.half.TBPHS = 119; // Gives a coarse phase shift from ePWM1 -> ePWM2 of 9°, or -351°
EPwm2Regs.TBPHS.half.TBPHSHR = 100; // Gives a fine phase shift of arbitrary value from ePWM1 -> ePWM2
EALLOW;
SysCtrlRegs.PCLKCR0.bit.TBCLKSYNC = 1;
EDIS;
I observe with this code that ePWM1 leads ePWM2 by 9°. It works the same as if I never configured any of the HR registers at all and only used the TBPHS.half.TBPHS for phase loading. Essentially, the high resolution seems to not be working.
Any help is sincerely appreciated. Thank you.
-Jeff