This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I'am using the LaunchPad Development Kit LAUNCHXL-F28379D with Matlab/Simulink. I want to use the two CAN modules but just one works.
The module eCAN_B works but the eCAN_A doesn't, I am using the same setting for both. I have tried with all of the pin assignment available without succeed. I have used an oscilloscope to measure the output from the driver to the transceiver and the output is always 3,3V.
Do I have to change other properties in order to enable the eCAN_A module?
Thanks in advance.
Regards,
Diego