Part Number: TMS320F28379D
Tool/software: Code Composer Studio
C28xx_CPU2: If erase/program (E/P) operation is being done on one core, the other core should not execute from shared-RAM (SR) as they are used for the E/P code. Also, CPU1 will be halted to determine SR ownership for the CPU which will run the Flash Plugin code, after which CPU1 will be set to run its application. User code execution from SR could commence after both flash banks are programmed.
C28xx_CPU2: Trouble Removing Breakpoint with the Action "Remain Halted" at 0xc0eb: (Error -1066 @ 0xC0EB) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 8.0.27.9)
C28xx_CPU2: Error executing PLL configuration algorithm. Operation cancelled. (0x0)
C28xx_CPU2: File Loader: Memory write failed: Unknown error
C28xx_CPU2: GEL: File: Y:\Software\Digital\IMPACT_FW\Series400\Firmware\Trunk\SecondaryCore\Bootloader\SantaCruzBootloader_LAN9252\Debug\SantaCruzBootloader_LAN9252.out: Load failed.
C28xx_CPU2: Trouble Setting Breakpoint with the Action "Remain Halted" at 0xc056: (Error -1066 @ 0xC056) Unable to set/clear requested breakpoint. Verify that the breakpoint address is in valid memory. (Emulation package 8.0.27.9)
C28xx_CPU2: Breakpoint Manager: Retrying with a AET breakpoint